Ultra-Mini ELECYLINDER® CE0297-1A
The modular Ultra-Mini ELECYLINDER® with a built-in controller can do big things! You can even keep spares in your pocket!
The modular Ultra-Mini ELECYLINDER® with a built-in controller can do big things! You can even keep spares in your pocket!
Move. Stop. Move. The Stopper That Works Non-stop. ELECYLINDER® Stopper Cylinders are ideal for conveyor stopper applications.
Cleanliness made easy with ELECYLINDER® Cleanroom Wide Sliders.
Need to move a 400kg horizontal payload at 2500 mm/s? We can handle it! IS(P)B is including ISB and ISPB models.
One of the components used in our R-Unit controller had an availability issue and there was a delay in delivery. Currently, the part that was difficult to obtain has a stable availability now and the delivery delay has been resolved.
The wide body is equipped with a built-in ball circulating type linear guide. It is most suitable for heavy workpieces and large overhang applications.
We will discontinue production of the IK series (RCP2 combination / RCS2 combination) in April 2023. We apologize for any inconvenience that this may cause.
We will discontinue production of the IX-NNN1205 / 1505 / 1805, IX-NNC1205 / 1505 / 1805 in April 2023. We apologize for any inconvenience that this may cause.
We will discontinue production of the RCS2-SA7 / SS7 / SS8 / RA5, RCS3–SA8 / SS8 in April 2023. We apologize for any inconvenience that this may cause.
A new rod type ELECYLINDER® is available with a Ball Bush Double Guide. Lifting and pushing have never been this easy.
Find Your Control: Download the latest Controller Reference General catalog.
The 2021 General Technical Reference Catalog is available to download.
We will discontinue production of the RCL-SA5L / SM5L in June 2022. We apologize for any inconvenience that this may cause.
Move over air hoses. Make some space for the ELECYLINDER®. Download the latest ELECYLINDER® General catalog.
The IFA belt driven actuator’s high speed capability combined with high acceleration allows for short cycle times.
The EC-ST15ME low-cost stopper cylinder is now available. – Workpieces up to 50kg. – Maximum collision speed of 9kg workpiece: 40m/min.
The IAI Robot Lineup Guide has been updated. We’ve added new EC cleanroom sliders, large sliders, a gripper, RCP6 Pulse Press, and a long arm SCARA.
A new, high-speed cleanroom SCARA for assembling and handling applications in a clean environment.
Unit-connecting controllers allows a wide number of actuator and control method combinations. RCON, REC and RSEL
Large ELECYLINDER® Slider type with a longer stroke and operates at higher speeds. EC-S10(X), 13(X) and 15(X)
A pulse press is an actuator combining a stepper motor and load cell, capable of power control.
We have discontinued production of the PCON-CA/CFA Field Network Controller in October 2021. The replacement model is the PCON-CB/CFB.
New gripper type actuators have been added to the ELECYLINDER® series. EC-GRB8, EC-GRB10 and EC-GRB13
A new ultra-large, high payload SCARA robot has been added to the IXA High-speed SCARA series.