West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

Cosmetics & Chemicals

10. Shampoo bottle filling equipment

10. Shampoo bottle filling equipment

The speed can be changed during movement, allowing the nozzle tip to move in accordance with the rate of rise of the liquid surface. By adjusting acceleration and deceleration, shampoo foaming can be prevented.

read more
Application Example: EC – Hand cream dispensing device

Application Example: EC – Hand cream dispensing device

System Overview : Improvement Overview : Device for filling containers on a conveyor belt with hand cream.An ELECYLINDER is employed to synchronize the dispensing device and the conveyor belt.Reduced labor cost of $10,560 per year thanks to shorter cycle...

read more
EC – Transfer System for Boxing Cosmetic Bottle

EC – Transfer System for Boxing Cosmetic Bottle

Mechanism for pushing boxes onto the next conveyor connected perpendicularly to the current conveyor An air cylinder was used to transfer packages containing cosmetic bottles between conveyors (connect-ed perpendicularly). However, sometimes the packages fell down due...

read more
EC – Deburring Device for Plastic Molding Products

EC – Deburring Device for Plastic Molding Products

A device to perform deburring of inside of lipstick caps. In the past, an air cylinder was used to load parts from the conveyor to the deburring machine and put them back on the conveyor after processing. However, it was not possible to shorten the cycle time because...

read more
EC – Sorting Device for Cosmetics on the Conveyor

EC – Sorting Device for Cosmetics on the Conveyor

A device for swaying a conveyor to sort cosmetic products into two lines for inspection machines. Two inspection machines are installed to enhance the inspection capacity. An ELECYLINDER® is used to sway a conveyor to divide the cosmetic products into two lines for...

read more