Inspection & Test
EC-15. Instant soup package sorting, Vision inspection for crushed boxes & missing prints
Compact slender type with built-in controller and shortened overall length. Wireless teaching is possible by using the teaching tool TB-03 or Wireless Teaching Controller.
EC-16. Circuit board reverser equipment
Rotary type also has adjustable acceleration and deceleration, allowing the speed to be increased while minimizing the impact of reversal.
01. Insert missing parts inspection equipment for resin cases
The inspection camera is brought to a smooth standstill by adjusting acceleration and deceleration. This can significantly reduce standby time due to camera vibration.
02. Tensile testing of wire harnesses – Pulse Press Electric Actuator
Pulse Presses can handle loads in the tensile direction and have no limit on tensile time. High precision judgments are possible at a low cost.
05. Automotive connector inspection equipment – Alternative to Vertical Articulated Robot
Diagonal approaches and tip swiveling, possible until now only with vertically articulated robots, can now be performed at a low cost. The wrist unit is capable of interpolating motion with the orthogonal axes.
17. Circuit board inspection inter-process transfer equipment – Belt-driven, Long-stroke
The belt-driven type is ideal for long-distance interprocess transfer because there is no speed reduction due to strokes. Stroke up to 3200mm, max. speed up to 3000mm/s.
Application Example: EC – Visual inspection of toilet paper
Replacing an air cylinder with an ELECYLINDER for removing and discharging defective products to the discharging conveyor belt.
EC – Transfer Device for Electronic Parts
A visual re-inspection process for rejected parts after a vision-camera inspection.Previously, this process was done manually all by hand (stretching hands to take the part, performing a visual inspection and returning the part). Depending on the workers' physical...
EC – Inspection Device of Bearing Torque
A device for inspecting bearing torqueWith the air cylinder, the speed and acceleration / deceleration were unstable, and there was a defect where the bearing was damaged by the impact of the holding jig. The ELECYLINDER® provides smooth deceleration, exerts no impact...
EC – Lifting Device of Semi-Finished Products for inspection
A device for lifting semi-finished products during assembling to perform a visual inspection of wiring on the bottom.Lifting up is required because the semi-finished product during assembling cannot be slanted for a visual inspection on the bottom. The ELECYLINDER®...
EC – Inspection Device for Substrate Continuity
A device for inspecting continuity of substrates by using a probe.In the past, an air cylinder was used. However, safety circuit designing for emergency stops (residual voltage, inadvertent leaping out, etc.) and restoring procedures after emergency stops were very...
EC – Door Opening for High-Voltage Inspection Device
A device for opening the door of a voltage inspection device for automobile electronic parts.From the designing stage, the inspection device was presupposed to employ an ELECYLINDER®. The following effects were confirmed: 1) Opening: high speed operation. Closing:...