Inspection & Test
Application Example – Air Cylinder was upgraded to ELECYLINDER – Shampoo Pack Defective Product Sorting Process
The inspection camera is brought to a smooth standstill by adjusting acceleration and deceleration. This can significantly reduce standby time due to camera vibration.
EC-15. Instant soup package sorting, Vision inspection for crushed boxes & missing prints
Compact slender type with built-in controller and shortened overall length. Wireless teaching is possible by using the teaching tool TB-03 or Wireless Teaching Controller.
EC-16. Circuit board reverser equipment – Transferring, Turning Around, Inspection, Turning Over, – EC Rotary and Mini Rod
Application Example – Circuit board reverser equipment – Transferring, Turning Around, Inspection, Turning Over – EC Rotary type and Mini Rod type
01. Insert missing parts inspection equipment for resin cases
The inspection camera is brought to a smooth standstill by adjusting acceleration and deceleration. This can significantly reduce standby time due to camera vibration.
02. Tensile testing of wire harnesses – Pulse Press Electric Actuator
Pulse Presses can handle loads in the tensile direction and have no limit on tensile time. High precision judgments are possible at a low cost.
05. Automotive connector inspection equipment – Alternative to Vertical Articulated Robot
Diagonal approaches and tip swiveling, possible until now only with vertically articulated robots, can now be performed at a low cost. The wrist unit is capable of interpolating motion with the orthogonal axes.
17. Circuit board inspection inter-process transfer equipment – Belt-driven, Long-stroke
The belt-driven type is ideal for long-distance interprocess transfer because there is no speed reduction due to strokes. Stroke up to 3200mm, max. speed up to 3000mm/s.
Application Example: EC – Visual inspection of toilet paper
Replacing an air cylinder with an ELECYLINDER for removing and discharging defective products to the discharging conveyor belt.
EC – Transfer Device for Electronic Parts
A visual re-inspection process for rejected parts after a vision-camera inspection.Previously, this process was done manually all by hand (stretching hands to take the part, performing a visual inspection and returning the part). Depending on the workers' physical...
EC – Inspection Device of Bearing Torque
A device for inspecting bearing torqueWith the air cylinder, the speed and acceleration / deceleration were unstable, and there was a defect where the bearing was damaged by the impact of the holding jig. The ELECYLINDER® provides smooth deceleration, exerts no impact...
EC – Lifting Device of Semi-Finished Products for inspection
A device for lifting semi-finished products during assembling to perform a visual inspection of wiring on the bottom.Lifting up is required because the semi-finished product during assembling cannot be slanted for a visual inspection on the bottom. The ELECYLINDER®...
EC – Inspection Device for Substrate Continuity
A device for inspecting continuity of substrates by using a probe.In the past, an air cylinder was used. However, safety circuit designing for emergency stops (residual voltage, inadvertent leaping out, etc.) and restoring procedures after emergency stops were very...