Tube, Pipe, Rod & Building Materials
Ultra-Large Slider Series EC-S18(X)LFR (Vertical Payload: 120kg) adopted for Lumber Vertical Lift – ELECYLINDER®️
Application Example: Lumber Vertical Lift Transport – A Ultra-large Slider is adopted – New Models with 120kg vertical payload – EC-S18(X)LFR
EC – Stocker for Flooring Panels
A device to transfer flooring panels from the feed conveyor to stockers. An air cylinder was used previously. As the speed increased, shocks also became bigger at the stroke ends, allowing the ooring panels to budge occasionally and preventing panels from stacking in...
Easy Automation Concept Vol.10 Videos
Example Video #19: System for inspecting/transferring stud bolt material - Air cylinder vs IAI's ROBO Cylinder A simple system configuration to reduce the cycle time by 44%. Material, round bars, are checked for outer diameter before a process of rolling machine....
Easy Automation Concept Vol.1-2 Video #02
Example Video #02: Equipment for polishing iron pipe interiors - Air Cylinder vs IAI's ROBO Cylinder (Japanese version) Equipment for polishing iron pipe interiors This is equipment for polishing the interiors of iron pipes with a brush. Point 1: Defective rate...
Architectural Aluminum Cutting Equipment Example
Cutting Cords to Variable Specified Lengths – CT-Effects Application Example
Motorizing the feed process increased production, and significantly lowered electricity and labor costs. Papers/Films/Wires/Building Materials Cutting Cords to Variable Specified Lengths - CT-Effects Application Example [ Robot/Electric Actuators ] RCP5-RA6C [Issues...
Applying a Liquid Solution to a Copper Twisting Machine
Changing an air cylinder to ROBO Cylinder improved the cycle time for the solution application process. Papers /Films/Wires/Building Materials Changing an air cylinder to ROBO Cylinder improved the cycle time for the solution application process - CT-Effects...
External Diameter Measuring Tool for Precision Pipe – CT-Effects Application Example
Inspected pieces: 585 pieces ⇒ 1,260 pieces (Increased by 675 pieces) Productivity Improvement of Approx. 115% Electronic Components External Diameter Measuring Tool for Precision Pipe - CT-Effects Application Example Here you can create the content that...
Medical Needle Cutting Application
Medical Needle Cutting Application – an slider actuator is used to feed needles to a cutting wheel so they can be cut to length – IAI America Application Example
Baseball Bat Inspection Application
IAI ROBO Cylinder has been adopted as an equipment that measures the shape of a baseball bat – Electric Actuator Application Example with animation
Aluminum Cutting Machine Application
ROBO Cylinder RCP2 is used to feed aluminum into machine to be cut – Touch panel is used to set the size and configuration of the aluminum to be cut – IAI Electric Slider Actuator