Paper, Film, Fabric, Glass & Board
Application Example Animation: ROBO Pump Catalog – Cardboard Printer
Application Example for new product, ROBOPUMP (ROBO Pump) – Kraft Paper Printing System – picks up via suction, transported to the printing unit and released.
Application Example: EC – Visual inspection of toilet paper
Replacing an air cylinder with an ELECYLINDER for removing and discharging defective products to the discharging conveyor belt.
EC – Feeding Device of Paper Carton Materials
A device for feeding paper carton materials to the next process.The workpieces (before formed into paper liquid packs) stacked by the ELECYLINDER® are lifted up to the predetermined position. The sensor detects the top of the stacked workpieces and stops the lifting....
EC – Panel Positioning Device
A device for adjusting the transfer position of panels which are flowing on the conveyor.The worker pushes the panel flowing on the conveyor against the stopper for positioning. Drilling is carried out in the next process. The stopper is used to change the stopping...
EC – Inspection Device for Glass Substrates
A device to perform a sampling inspection of glass substrates. This device performs a sampling inspection for glass substrates. The ELECYLINDER® transfers the glass substrate, while the cameras perform an inspection from the top and bottom simultaneously. The customer...
EC – Positioning Device for Glass Substrates
Adjusting the distance between guide plates of a transfer device according to two sizes of glass substrates. This device is to adjust the distance between two guide plates according to the size of the glass substrates in order to regulate the transfer position in a...
Sending Defective Products to the Removal Line
Industry: Others Process: Sorting, Inspecting Actuators: RCP5-SA7C Motorizing the removal of defective products made high speed possible and lowered costs. [Issues Until Now] An air cylinder was used for the movement of the plate that removes defective products....
Easy Automation Concept Vol.3-2 Video #06
Example Video #06: Sequential Feeder for Non-woven Fabric Punching Line - 10 Air cylinder vs 1 IAI's ROBO Cylinder The sequential feeder, a part of a press machine that punches out non-woven fabric for filters. The press machine performs punching operation at specific...
Film Feeder for Packaging Machine – Application Example
Industry: Paper, film, construction material Process: Cutting Actuators: RCS2-SA7C-A-60-16-900 x2 In a packing machine, ROBO Cylinder was adopted for equipment that cuts packaging film to a set length. As shown in the illustration above, two ROBO Cylinders are used to...