| [ Robot/Electric Actuators ] |
[ Controllers ] |
| RCP3-SA4 | MEC Controller |
Robo cylinders and MEC controllers have been adopted as devices that apply adhesives with mechanical dispensers to mechanical parts.
It is a semi-automatic device that moves the dispenser left and right by using only operation switches without using PLC. When the work type changes, the stop position and the speed are changed in the teaching box CON-PT.
In the past, an air cylinder was used, and when the workpiece was changed, the position of the stopper was changed each time to change the application position. It took time and effort because there were many types of workpieces. The Robo Cylinder + MEC makes it easy and accurate to change the settings. In addition, since air is not used, the compressor becomes unnecessary, and the system becomes simple.