West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

Rotary Selection Method

When selecting a rotation axis, it is necessary to calculate the moment of inertia of the condition to be used and to use a model that allows the moment of inertia.
Please calculate the moment of inertia of the work to be used and the mounting jig by calculating the moment of inertia of the representative shape shown below. (Please refer to the correlation diagram of the shape and mass of the attached item is posted on the next page.)
In addition to the allowable moment of inertia, it is also necessary to check the load moment. Please select the model that can tolerate the moment generated from the shape and size.

▶ PDF of this topic

▶ GO TO Full Technical Reference Catalog
Shares
Share This