West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

Reference for Setting the Speed of SCARA Robot IX

SCARA robot IX can not operate continuously at maximum acceleration / deceleration and maximum speed of the catalog. When operating at maximum acceleration / deceleration, please set stop time referring to the reference graph of continuous operation duty.
When continuous operation is required, please operate with the acceleration / deceleration setting of the continuous operation guide range of the reference graph of acceleration / deceleration setting.

▶ PDF of this topic

▶ GO TO Full Technical Reference Catalog