West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

Mini Rod Type Anti-Rotation Installation Method

■ Thin and small rod type anti-rotation
In the following models, there is no anti-rotation of the ball screw inside the main body, so be sure to set the anti-rotation on the outside when using. When installing the anti-rotation, please install according to the following installation conditions. If you operate in a state where the anti-rotation mechanism is not installed, the ball screw idles, the rod does not move back and forth, and the rotation speed of the encoder and the actual movement distance can not be matched and the position may be misaligned.

▶ PDF of this topic

▶ GO TO Full Technical Reference Catalog