West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

IF Series Motor Installation Orientation

Depending on the installation condition of the actuator, the positions of the motor and sensors can be changed to 6 types as shown below.
This makes it possible to change the motor position according to the installation environment.
Where the motor is installed horizontally or below, the position of the motor will be lower than the slider so there is no work interference.
In addition, when attaching the creep sensor (C) and the origin limit switch (L) as an option, when the motor installing direction is L, they are mounted as standard (on the right side as viewed from the motor side, symbols C and L). R they are mounted to the reverse side (on the left side as viewed from the motor side, symbols CL and LL).

▶ PDF of this topic

▶ GO TO Full Technical Reference Catalog
Shares
Share This