West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

Diagrammatic Representation of Plane Surface

 Extracted from JIS B0031 (1994)

■ The position of each instruction symbol with respect to the instruction symbol in the figure

Instruction marks related to the skin of the face are obtained by placing the value of the surface roughness, the cutoff value or the reference length, the processing method, the mark of the line direction, the surface waviness and the like at the position shown in FIG. 1 Represent

▶ GO TO Full Technical Reference Catalog
▶ Click to open PDF of this topic