Ballscrew Accuracy
The lead accuracy of our company's ball screw is equivalent to the accuracy class C5 or C10 of JIS standard (JIS B 1192). The accuracy of C10 is defined as ± 210 μm for the typical transfer amount error (see figure below) for 300mm.
The accuracy of the C5 (the typical transfer amount error and the allowance value of the variation) is as follows.
Note: The numbers in the table below are reference values, and absolute positioning accuracy is not guaranteed.