Food & Beverages
Application Example: EC – Device for extruding cheese
Device for extruding cheese and cutting into string-like thin shapes. Replacing an air cylinder with an ELECYLINDER for extruding cheese.
Application Example: EC – Door opening device
System Overview : Improvement Overview : Device for opening a door at a transfer process of cardboard boxes to the shipping platform.Replacing an air cylinder with an ELECYLINDER ® for opening the door.Annual cost reduction of $1,680 by adjusting...
Application Example: EC – Device for putting syrup on doughnuts
Device for putting syrup on doughnuts on a conveyor belt. Replacing an air cylinder with an ELECYLINDER ® to move and dispense syrup.
Application Example: EC – Device for transferring short cakes
System Overview : Improvement Overview : Device for transferring packaged short cakes to the next process conveyor belt.Replacing an air cylinder with an ELECYLINDER to transfer packaged short cakes.Reduced labor cost of $7,800 per year thanks to the shortened...
EC – Transfer Device for Breads
A device for transferring breads on the tray transfer conveyor.When breads are fed out to the transfer conveyor before filling the tray, the transfer timing has to be adjusted by using a stopper. The ELECYLINDER® can easily adjust the starting/stopping positions and...
EC – Transfer Device for Stacked Frozen Food Packs
A device for stacking and transferring frozen food packs to the conveyor of the next process.This device transfers frozen gyoza dumplings from the wrapping process to the next process of packing into cardboard boxes. Packs are dropped from the conveyor by free fall,...
EC – Feeding Device of Paper Carton Materials
A device for feeding paper carton materials to the next process.The workpieces (before formed into paper liquid packs) stacked by the ELECYLINDER® are lifted up to the predetermined position. The sensor detects the top of the stacked workpieces and stops the lifting....
EC – Flattening Device for Chocolate Surface
A device for flattening chocolate surface after filled into a die. When flattening chocolate, an air cylinder transferred its vibration to the flattening bar at the time of stoppage. It made waves on the chocolate surface, but adjustments were difficult. By employing...
EC – Centering Device for Beverage Paper Packs
A device for centering beverage paper packs on a conveyor. Previously, air cylinders were used to align beverage paper packs in the center. Air pressure adjustments (to prevent the packs from being smashed) after a periodical maintenance was difficult. The employment...
EC – Sorting Device for Instant Soup Packages
A device to inspect instant soup packages (visual examination), and sort them into two locations. In the past, air cylinders were used at the sorting gates to move the gates vertically. Quality products were sometimes flicked off the conveyor due to a shock at the...
EC – Mixing Device of Sauce into Food Ingredient
A device to evenly mix sauce dispensed from a nozzle into an ingredient container. An ELECYLINDER® has been employed to add sauce into ingredient for mixing them evenly by waving the nozzle from side to side. It enables sauce to mix evenly and quickly. EC-S6 ...
EC – Aligning Device for Lunch Boxes on a Conveyor
A device to align lunch boxes on the conveyor before a packaging machine. The ELECYLINDER® rod type pushes on the guide plate the lunch boxes that are flowing on the conveyor, and aligns them before going into a packaging machine. Previously an air cylinder was used,...