Diagrammatic Representation of Plane Surface
Extracted from JIS B0031 (1994)
■ The position of each instruction symbol with respect to the instruction symbol in the figure
Instruction marks related to the skin of the face are obtained by placing the value of the surface roughness, the cutoff value or the reference length, the processing method, the mark of the line direction, the surface waviness and the like at the position shown in FIG. 1 Represent