West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page


IAI Electric Actuator Application Examples

 
Medical
medical needle cutting application in automation with IAI electric actuators
Medical Needle Cutting Application

Video from IAI YouTube Channel:

Actuators
RCAW-RA4R, ISPWA-S
Controller
ACON, SCON
 
  • ISPWA actuator is used to feed needles to a cutting wheel so they can be cut to length.
  • RCAW actuator is used as an elevator to raise and lower the cutting wheel at a constant low speed.
  • Traditionally, the needles were fed by using an air cylinder and a hydraulic cylinder was used to actuate the cutting wheel.

The following advantages are achieved by using the electric actuators:
 
1. The setup is easy to change.
2. Better speed control in raising and lowering of the cutting wheel achieves better accuracy and results in an improvement of the quality of the cut surface.
 
 

Back to IAI electric actuator application examples

See the energy efficient ROBO Cylinder Electric Actuator Lineup

ROBO Cylinder Electric Actuator Visual Index