West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

 

Inspection / Examination / Etc.
LED Light Inspection Application Example
Actuator: RCP4-SA5C
Controller: PCON-CA
  • The ROBO Cylinder has been adopted into a machine for measuring the intensity of the LEDs which are placed at regular intervals inside the LED fluorescent shape lamp.
  • To measure the illumination, the slider moves a light meter to each interval of an LED. The measurement results are managed by a personal computer.
  • Traditionally, the measurements were conducted manually and there was a variation in the measurement position. By adopting the ROBO Cylinder, the accuracy of the measurement position has been improved.
  • In addition, by automating, the measurement efficiency was also improved by being able to simultaneously measure three LED fluorescent shape lights at a time.