West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page
Mechanism for pushing boxes onto the next conveyor connected
perpendicularly to the current conveyor
An air cylinder was used to transfer packages containing cosmetic bottles between conveyors (connect-ed perpendicularly). However, sometimes the packages fell down due to shocks and deformed or allowed the liquid in the bottles to foam up.
With the new ELECYLINDER® system, we can easily adjust and control AVD (A: acceleration, V: velocity, D: deceleration) to make sure the packages are smoothly transferred between the conveyors without affecting the products inside.
Shares
Share This