West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

EC – Sorting Device for Medicine Packages

A device for sorting medicine packages by scanning printed data on the package surface.
Previously, an air cylinder was used to transfer accepted products. To achieve a shorter cycle time, the air cylinder was operated at a high speed, but gave a big shock at the time of stoppage. As a result, some temporary stops took place in the post-process due to the dispersion of transferred positions of accepted products.

Since the ELECYLINDER® can adjust acceleration/deceleration, there is no shock even at a high speed operation.
As a result, the dispersion of the transferred positions was eliminated, reducing temporary stops and shortening the cycle time.