West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

EC – Sorting Device for Cosmetics on the Conveyor

A device for swaying a conveyor to sort cosmetic products into two lines for inspection machines.
Two inspection machines are installed to enhance the inspection capacity. An ELECYLINDER® is used to sway a conveyor to divide the cosmetic products into two lines for feeding.
Previously an air cylinder was used, which was the bottle neck because the speed could not be increased due to large shocks at the time of stoppage.