EC – Device for Inserting Metal Parts into Plastic Bases
This device inserts a metal part into a plastic base frame in an electronic part assembling process.

When inserting a metal part, it is necessary to slow down for the last 1mm. For this reason, a spring was used at the tip of an air cylinder for the insertion process.
Some defects were observed when the spring deteriorated over time.
Some defects were observed when the spring deteriorated over time.
The ELECYLINDER® can control D (deceleration), allowing positioning at a low speed and indication of an error when stopping (defective products) before the forward end. Since the ELECYLINDER® needs no spring, there are no defects caused by the deterioration of the spring.