West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page
No Specific Industries
Alignment of the Resin Block Application Example
Robots: RCA2-TWA4NA, RCS2-TWA5N
Controllers: ACON, ASEP, MSEP, SCON
  • In a system for performing the alignment of some resin blocks, the ROBO Cylinder was adopted. The company’s products include designer plates to be used on the floor of a house by bonding resin blocks.
  • Previously, an air cylinder was used, this was changed to ROBO Cylinder which improved the cycle time and reduced the occurrence of Choco-Tei events.
  • When air cylinder was used
    Because the resin blocks were misaligned by the impact of the air cylinder stop, they were operating it at a reduced speed. However, Choco-Tei was still occurring about 10 times a day because of the misalignment due to unstable speed. To rearrange the resin block and to recover from Choco-Tei, it took about 1 minute.
  • After changing to ROBO Cylinder
    By replacing air cylinder to ROBO Cylinder, and adjusting the pressing force and acceleration/deceleration, they could increase the operating speed while minimizing the impact at the time of stop. In addition, Choco-Tei was reduced to near zero.

Reduction in Cycle Time/Choco Tei — CT Effects
Align resin block table1
Align resin block table2
 

Shares
Share This