West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

Ct effects logo

Production Amount per Day:
560 ⇒ 940 pieces: ⇒  Productivity Improvement of 68%

 

Electronic Components / Applicator
Adhesive Applicator - CT-Effects Application Example
[ Robot/Electric Actuators ]
[ Controllers ]
RCP2-SA7C (2 axes) PSEL
RCP2-RA10C PCON-CFA
ISB-MXL XSEL

 

  • [Equipment Overview]
    An apparatus for applying an adhesive to the cover of lamp lights and an indicator light in the manufacturing of electronic components.

    X-axis: RCP2-SA7C
    Y-axis: RCP2-SA7C
    Z axis: ISB-MXL
    Dispensing of the adhesive: RCP2-RA10C

 

  • [Problems of the air cylinder used]
    1. They were dispensing the adhesive by using the air cylinder. The dispensing rate was changed because the air pressure was unstable and the adhesive was interrupted or lumped.
    2. The viscosity of the adhesive changes under the conditions such as temperature, so that it took time to adjust the dispensing pressure.
    3. Defective parts were made when the adhesive that attached to the work parts formed adhesive strings that weren’t cut off after dispensing.

 

  • [Benefits of the electric actuator]
    • The 45 seconds cycle time has been reduced to 30 seconds because the amount of adhesive dispensed always stayed stable.
    • This enabled the supply of adhesive to be stable all day after trial testing each morning.
    • The failure rate due to adhesive dispensing reduced to almost zero from about 10 pieces a day since they set movement to cut clean the dispensed adhesive. This movement was of the electric actuator in the vertical direction and the slide table.

 

[CT Effects - Reduction in Cycle Time/Choco Tei]

 

Project Comparison Equipment with the air cylinder Equipment with the ROBO Cylinder
Cycle Time 45 seconds 30 seconds
Duration of Choco-Tei per event 60 minutes / day 60 minutes / day
Production per day 560 pieces (*1) 940 pieces (*2)

(*1) When the air cylinder was used: (8 hours - 1 hour Choco-Tei) ÷ 45 seconds = 560 pieces per day
(*2) When the ROBO Cylinder was used: (8 hours - 10 minutes) ÷ 30 seconds = 940 pieces per day

See more IAI electric actuator application examples