West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

Types of Linear Electric Actuator (Single Axis)

Feature and Usage Categorized by Types of Linear Electric Actuators
 

 A       Slider type

 Features    

  • The slider on the top of the main unit works in the shape of a standard electric actuator.
  • Workpiece can be attached by using the tapped holes provided on the slider.
  • It has a built-in linear guide with the base integrated ball circulation model, which increases the moment of pitching, yawning, and rolling directions.
[ New technology ] Arrival of Wide slider type!
  • The adoption of the wide body allows the allowable load moment up to 14 times more compared to the standard slider type.
  • It is suitable for usage with large overhanging. If a standard linear actuator with an external guide is being considered, the wide slider type can replace both of these in one.

1 109 80kg 2 1
(RCP6-WSA16C's allowable moment load example: offset 500mm with 80kg)

 Usage    

  • It is suitable for usage where workpieces are placed on sliders and for positioning purposes.
  • Ideal for replacing the rodless air cylinders or internally produced equipment that is combined with ball screws + guide + motors.
  • Ideal for base axis / moveable axis for orthogonal combinations.
  • It can be used for usage requiring accuracy, such as the feed mechanism of the camera in the inspection process and the measurement with a laser displacement meter.

Model Selection Flow Diagram - Slider / Linear Servo

When customers say, "We wish this existed," we make it happen.

2024GEN 3kan 003 004 EN Page 1 connected

Selection from Stroke and Payload - Slider / Linear Servo

When customers say, "We wish this existed," we make it happen.

* Some phones/tablets might not properly display the PDF on this webpage.
Please use a download link if you would like to have the full-page PDF.

Please use scroll bar to see more pages.
Shares
Share This