West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

EC – Door Opening for High-Voltage Inspection Device

A device for opening the door of a voltage inspection device for automobile electronic parts.
From the designing stage, the inspection device was presupposed to employ an ELECYLINDER®. The following effects were confirmed:

1) Opening: high speed operation. Closing: easy adjustment for slow speed.
2) Four identical devices were manufactured. The same setting (values) were copied from the first one to the second one onwards, allowing quick start-ups.
3) Only electricity is used. No air source or piping is needed.
4) The light curtain makes the operation stop immediately, ensuring safety.