The key to reducing production costs is found in CT effects.
So what exactly are CT effects?





Reduction of Cycle Time


Overview of the Line

This case example involves onboard assembly and test lines with four steps. The cycle time of Step 3, which was taking the longest among them, was reduced.

Line Overview

System specifications

  • Number of air cylinders = 8 units
    • Unit 1 - Moves the work table
    • Unit 2 - Press-fitts the connector
    • Unit 3 - Electric continuity test
    • Units 4, 5, 6 - Stamping
    • Unit 7 - Connection of wires for inspection
    • Unit 8 - Stops the work table at the midpoint

  • Product types supported = 10 types (25 types can be supported with 3 lines.)
  • Cycle time = 14.0 seconds


Overview of the System

It is a simple semi-automatic system that conducts a performance test of onboard sensors. When the operator sets the work part and presses the start switch, the work table moves forward toward the back of the system. Once steps 1, press-fitting of the connector (assembly): 2, electrical continuity test: and 3, stamping (PASS stamp) are completed, the table comes back to the forward position.




Significant Improvement of Production Efficiency through Motorization


With the air cylinder system, the work table could not be operated faster because it would have increased the shock upon stopping. With the ROBO Cylinder system, on the other hand, the maximum speed can be increased because the actuator stops without generating shock. In addition, the ROBO Cylinder system starts quicker than the air cylinder system, which enabled significant reduction of the cycle time.
Work table operation takes 1.8 seconds less.



With the air cylinder system, an automatic switch was used to determine whether the work part had been pressed to the specified position, which made the operation unstable and required 4 seconds for the press-fitting action to ensure quality. With the ROBO Cylinder system, on the other hand, push-motion operation can be performed using the zone function and consequently the press-fitting time was successfully reduced by 2 seconds.
Push-motion operation takes 2 seconds less.






Number of lines and operators required to produce
5,000 pieces in one 7.5-hour day (27,000 sec.)

Air cylinder system ROBO Cylinder system
Cycle time 14.0 sec. 10.2 sec.
Number of work parts that can be
produced per line in one 7.5-hr day (27,000 seconds)
27,000 seconds / 14.0 seconds = 1,929 pcs 27,000 seconds / 10.2 seconds = 2,647 pcs
Number of lines required 5,000 pcs / 1,929 pcs =
2.6 -> 3 lines
5,000 pcs / 2,647 pcs =
1.9 -> 2 lines
Number of operators required (one operator per line) 1 operator x 3 lines = 3 operators 1 operator x 2 lines = 2 operators



Other Conditions

Air cylinder equipment cost for one unit $55,600
ROBO Cylinder equipment cost for one unit $61,100
Labor cost for one person $72,200/year



Increased Profits through Motorization

Year 1 Equipment cost: Reduced from 3 to 2 lines
Labor cost: Reduced from 3 to 2 operators
$55,600 x 3 lines – $61,100 x 2 lines = $44,600
$72,200 x (3 - 2 operators) = $72,200 x 1 = $72,200
__________________________________________
Sub-total: $116,800
Year 2 Labor cost: Reduced from 3 to 2 operators $72,200
Year 3 Labor cost: Reduced from 3 to 2 operators $72,200
3-year total: $261,200

As illustrated above, the reduction of cycle time through the motorization of the air cylinder system yielded a profit of $116,800 for the first year, and $72,200 for the second and subsequent years, resulting in a 3-year total of $261,200.



mautic is open source marketing automation
Get Our Monthly Newsletter

Get Our Monthly Newsletter

Subscribe to IAI Actuator News to receive monthly updates and tips.

You have Successfully Subscribed!