West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page

Ct effects logo

Labor Cost Reduction ⇒ $9,000/year

One operator
*Labor $18.00/hour 8 hours/day
*Overtime work 2 hours
*250 operational days/year

*Exchange Rate: 1(USD)=100(Japanese Yen)

 

Electronic Components 
Continuity Inspection Tool - CT-Effects Application Example

Here you can create the content that will be used within the module.

[ Robot/Electric Actuators ]
[ Controllers ]
RCP4-SA7C,   RCP2-SS8C PCON-CA

 

  • [Equipment Detail]

    It is a continuity inspection tool used for a PC extension board manufacturer.

    An air cylinder is used in this application to insert an edge connector on a PC board.

    An operator loads and unloads a PC board to the air cylinder manually.

 

  • [Problems in Using an Air Cylinder]


    Since you can’t change speed with air cylinders, you will need to move the entire stroke at the same speed to insert the PC board to the inspection tool. The cycle time is 15 seconds, and the number of work pieces that can be inspected in an 8 hour work day was 1,920 pieces *1.

    Management decided to increase the production volume of the PC boards to 2,400 pieces per 8 hour shift and to accomplish this, 2 hours *2 of over time per day was required.


    *1 (8 * 60 * 60) seconds/ 15 seconds/ piece

    *2 (2,400 – 1,920) pieces * 15 seconds/ piece

     

    [Benefits of Replacing with ROBO Cylinder]

    By switching to ROBO Cylinder, this enables them to move at high speed before insertion and then slow down just before the insertion, which lead to a shorter cycle time of 12 seconds. 

    It is now able to finish inspection within the operational hours. Also the reduction of labor cost for overtime work was accomplished.

    The cost spent to replace the cylinder was retrieved in the 1st year, which resulted in a cost reduction of $9,000 from the 2nd year.

     

[CT Effects - Reduction in Cycle Time/Choco Tei]

 

Subject Equipment with Air Cylinder Equipment with the ROBO Cylinder
Cycle Time 15 seconds 12 seconds

 

See more IAI electric actuator application examples