IAI

Reference:How to download/save CAD

・ There are several ways to save CAD data through Web browsers.
・ We will explain using Internet Explorer 6 as an example here. Please refer this if you have problems with saving the file.
・ Even if you are using other Web browsers, please perform the operation in the same procedure.

1. Save in accordance with the instructions on the Web browser by right-clicking on "DXF"




2. In case the extension of the saved file is garbled...
・ If the extension is saved garbled in ".txt" or " .dat"...
Please rewrite the extension to " .dxf" after saving, and then open file in CAD.
・ If ".txt" is added in saved file name...

  Ex. : ******.dxf is saved as → ******.dxf.txt
Please delete an extra extension after saving, and then open file in CAD.

    ******.dxf.txt → ******.dxf