IAI Electric Actuator Application Examples
Application Examples with IAI Electric Actuators
| Automotive |
 |
| Wire Stripper |
|
|
| Actuators |
|
|
Controller
|
|
Note: Aside from having guides to support the vertical shear, guides should also be used to help support the actuator shaft from the moment load being imposed upon if from the wire being sheared.
|
- Wire coating equipment has adopted the ROBO Cylinder. The wire stripper moves in slowly at first and then moves back quickly.
- It is difficult to adjust an air cylinder since there’s the possibility of the copper wire inside to break and fly out
Process Explanation
- The stripper must be moved into position. Since the wire can be stripped to different lengths, a multipoint positioning feature is needed.
- The wire is positioned across the stripper covering the notch and is pulled slowly at first to prevent the copper wire from being cut. Then as soon as the coating is sheared, the stripper is moved quickly.
- The stripper can be slowly moved halfway to the end of the cable and then move quickly to the end. Speed changes like this can be done easily with the ROBO Cylinder.
|
Back to IAI electric actuator application examples
See the energy efficient ROBO Cylinder Electric Actuator Lineup

-- Download this page as a PDF --
Related posts:
- Ink Filling Application
- 3-axes Inspection Application
- Vision Inspection Conveyor System Application
- Positioning and Deburring Aluminum Application
- Baseball Bat Inspection Application