Press Fitting Sample Application


IAI Electric Actuator Application Examples

Application Examples with IAI Electric Actuators
Automotive
press fitting application in automation with IAI electric actuators
Press Fitting

Actuators
ROBO Cylinder RCS2-RA13R-I-625-50-750-M-T2
Controller
SCON-I-C-750-2-2-NP
  • In the process of assembling automotive parts, a press adopts a very high thrust type ROBO Cylinder to perform the operation.
  • A pressing jig is mounted to the cylinder.
  • Previously, an air & hydraulic press had been used. However, in this case, the customer was using three different types of jigs, and it was very troublesome to change the jig for every change in part.
  • The ROBO Cylinder was adopted and was easily reconfigured for each part. This effect was seen immediately following its introduction. The plant is now considering switching a group of 170 other presses to ROBO Cylinders.
Cycle Time shortened 2.84 seconds -> 1.79 seconds
Annual power consumption costs reduced $40.73 -> $13.65
Reduction of annual C02 emissions 88.2 kg-cc -> 19.7 kg-cc
Reduction of annual CO2 emissions if all air equipment in the plant was replaced 15t-cc -> 3.35 t-cc

Back to IAI electric actuator application examples

See the energy efficient ROBO Cylinder Electric Actuator Lineup

ROBO Cylinder Electric Actuator Visual Index




-- Download this page as a PDF --

Related posts:

  1. Green Automation: Automobile Part Press Fitting
  2. Adhesive Press Equipment for Electronic Parts Assembly
  3. IX SCARA Sample Application Videos
  4. Deburring Automotive Parts Application
  5. 3-axes Inspection Application