West 800-736-1712 | Central 800-944-0333 | East 678-354-9470
Select Page


IAI Electric Actuator Application Examples

 

Automotive
lathe application in automation with IAI electric actuators
Numerically Controlled Lathe

Video from IAI YouTube Channel:

Actuators
ROBO Cylinder RCP2W-RA10C
Controller
PCON-CF
 
Note: Proper precautions should be taken such that the actuator doesn't receive any rotational torques or lateral loading. This may be accomplished by mounting a bearing at the end of the rod and by properly centering the work piece.
 
 

  • In a NC (numerically controlled) lathe, a hydraulic cylinder is used to push the cylindrical center work piece into the chuck from the opposite side. The following problems may occur when using the hydraulic cylinder:
  •  
    1) When the work piece changes, this causes time-consuming setup changes
    - Workers must manually position the work piece and use an indicator to make sure it is properly centered.

    2) The pressure change is not subtle
    - The pushing force for the work piece can be too strong and can cause it to bend
    - In order to change the force, a reducing valve must be installed to change the pressure which is done by using a bypass circuit

  • However, by adopting the ROBO Cylinder, the setup is automated and thus makes the adjustment of the pushing force to the work piece easier.
  •  

Back to IAI electric actuator application examples

See the energy efficient ROBO Cylinder Electric Actuator Lineup

ROBO Cylinder Electric Actuator Visual Index

Shares
Share This