Food Packing Application


IAI Electric Actuator Application Examples

Application Examples with IAI Electric Actuators
Food Processing
food packing application in automation with IAI electric actuators
Food Conveyor Packer

Actuators
ISA-LYM-I-400-40-1200-T2-S
Controller
SSEL-C-1-400I-NP-3-1
Note: This is not an example of conveyor tracking
  • Packages of hot food flow on a conveyor towards heat bonding equipment to seal the lids
  • Traditionally, the conveyor stopped and allowed thermo-compression which produced quantities of 50 products per minute
  • With the switch to the ISA actuator, this allows the conveyor to run continuously
  • The production has roughly doubled to between 100~110 products per minute thereby doubling in efficiency
  • Therefore, extra production lines could be removed and thus saving floor space in the plant
  • This new system can respond to changes in production volume and is flexible

Back to IAI electric actuator application examples

See the energy efficient ROBO Cylinder Electric Actuator Lineup

ROBO Cylinder Electric Actuator Visual Index

Related posts:

  1. Food Processing Example Application
  2. Examples of Food Applications Cost Savings
  3. Example of Cosmetics Application Cost Saving
  4. Vision Inspection Conveyor System Application
  5. Dessert Placement Application