E-CON Error Codes & Descriptions

E-Con: includes E-Con, ROBO Cylinder RCP2, RCP, RCS, ERC, ERC2, SCON, PCON, ACON Controllers.

Error Cause Description
040 Emergency Stop Emergency stop status.
05A Transmission Error Abnormal Communication, Check for noise. Inspect all serial ports and cables involved.
05B Transmission Framing Error Abnormal Communication, Check for noise. Inspect all serial ports and cables involved.
05C Transmission Time Out Error Abnormal Communication, Check for noise. Inspect all serial ports and cables involved.
05D Start Text Error Abnormal Communication, Check for noise. Inspect all serial ports and cables involved.
05E End Text Error Abnormal Communication, Check for noise. Inspect all serial ports and cables involved.
061 FNCCHR, W Address Error Serial string needs to be formatted correctly.
062 1 Operand Error Incorrect Data Command (possibly an operation not allowed with the controller type).
063 2 Operand Error Incorrect Data Command (possibly an operation not allowed with the controller type). In case of another linked controller, there could be parameter data which exceeds 2000 rpm set by SW7 – ON, and SW8 – OFF located on against the controller. Incorrect Data Command Rejection (could be an operation not allowed with that controller type).
064 3 Operand Error Incorrect Data Command (possibly an operation not allowed with the controller type).
070 RUN-OFF, Transfer Command Execution Requirement Incompatible Command Rejection (possibly due to External POP command).
071 No Homing, PTP Execution Requirement Incompatible Command Rejection (possibly due to External POP command).
073 Servo ON, Error Reset Execution Requirement Incompatible Command Rejection (possibly due to External POP command).
074 Communication Error Execution Requirement Incompatible Command Rejection (possibly due to External POP command).
075 During homing, movement command Execution Requirement Incompatible Command Rejection (possibly due to External POP command).
07F BCC Error Abnormal Communication, Check for noise. Inspect all serial ports and cables involved.
0A2 Position Data Error Cause:
[1] Move command input when no target position data was set in the “Position” field
[2] The target position in the “Position” field exceeds a soft limit setting.
[3] An incremental target position was specified in the “Position” field in the 3-point type controller.
Action:
[1] Set a target position first.
[2] Change the target position to a value inside the soft limit setting.
[3] Specify an absolute target position (expand the position table view to see this column).
0B0 Bank 30 Error (Parameter) Execute a common parameter edit or initialize the controller.
0B1 Bank 31 Error (Point) When release is not possible with the controller power supplied, you will need to either execute a common parameter edit or initialize the controller. Also, this error occurs when you try to execute a point through I/O that does not exist.
0B7 Magnetic Pole Non-Confirmation When the servo is turned on for the first time after the power has been input, this controller performs magnetic-pole phase detection. This error indicates that the magnetic-pole phase cannot be detected after the specified time has elapsed.
Cause:
[1] The connector of the motor relay cable is loose or disconnected.
[2] The brake cannot be released on a controller equipped with brake.
[3] The motor is receiving a high load due to application of an external force.
[4] Large slide resistance of the actuator itself
[5] Large slide resistance of the actuator itself
[6] Power supply is insufficiently sized for the voltage/current required by the system.
Action:
[1] Check the wiring condition of the motor relay cable.
[2] Check the wiring condition of the brake cable, and also turn on/off the brake release switch to see if the brake makes “click” sounds.
[3] Check for abnormality in the assembly condition of mechanical parts.
[4] If the load is normal, cut off the power and move the actuator by hand to check the slide resistance. If the actuator is suspected to be the cause, please contact IAI.
0B8 Pole Sense Error This controller performs excited-phase detection when the servo is turned on for the first time after the power on. This error indicates that the specified encoder signal level could not be detected after excitation for the time set by parameter No. 29 (Excited-phase signal detection time).
Cause:
[1] Loose or disconnected motor-relay cable connector
[2] Brake cannot be released on a controller equipped with brake.
[3] Large motor load due to application of external force
[4] Power was input when the actuator was contacting a mechanical end.
[5] Large slide resistance of the actuator itself
Action:
[1] Check the wiring condition of the motor relay cable.
[2] Check the wiring condition of the brake cable, and also turn on/off the brake release switch to see if the brake makes “click” sounds.
[3] Check for abnormality in the assembly condition of mechanical parts.
[4] Move the actuator away from the mechanical end and then reconnect the power.
[5] If the load is normal, cut off the power and move the actuator by hand to check the slide resistance. If the actuator is suspected to be the cause, please contact IAI.
0B9 Communication Error 2. Check Make sure that the payload is within specification. Make sure that the external power source works well. Check the motor encoder cable.
0BA Homing Sensor not Found When homing , mechanic end is found before sensor was detected. Please check sensor, wiring.
0BE Homing Time Out Check physical connection of the motor and actuator. Actual movement may not be happening.
0BF Creep Sensor not Found Found home sensor or mechanic end before creep sensor was detected while homing. Check sensor, wiring and for mechanical binding.
0C0 Excess Speed Please reduce the payload and/or speed.
0C1 Servo Error This alarm indicates that after receiving a movement command the motor is unable to operate for two seconds or more before reaching the target position.
Cause:
[1] Loose or disconnected motor-relay cable connector
[2] Brake cannot be released on a controller equipped with brake.
[3] Large load due to application of external force
[4] Large slide resistance of the actuator itself
Action:
[1] Check the wiring condition of the motor relay cable.
[2] Check the wiring condition of the brake cable, and also turn on/off the brake release switch to see if the brake makes “click” sounds.
[3] Check for abnormality in the assembly condition of mechanical parts.
[4] If the load is normal, cut off the power and move the actuator by hand to check the slide resistance. If the actuator is suspected to be the cause, please contact IAI.
0C2 Over Run (servo) Find over run sensor. Please check the following:
• Exceeding of the valid stroke range by external force in the servo OFF status. (regular detection)
• Exceeding of the valid stroke range by a forward jog at incremental encoder system. (coordinate not settled) (regular detection)
• Exceeding of the valid stroke range due to connecting an actuator with a different lead from controller setting.
• Abnormal homing operation of Incremental encoder system. Or by absolute set positioning fault, coordinate is out of alignment. Therefore, it does not stop at soft limit and exceeds the valid stroke range.
• By soft limit setting fault, soft limit is set higher than the valid stroke limit. Therefore, it does not stop at the soft limit and exceeds the valid stroke range.
• Regardless of valid stroke length, due to abnormal sensor behavior & wiring, it is in the overrun sensor detection status.
• Regardless of valid stroke length, due to a sensor related parameter (use/not use, a contact/b contact) setting fault, it affects the overrun sensor detection
0C8 Overcurrent Motor circuit may have shorted, due to excessive load. This alarm will not clear unless you cycle power.
0C9 Excess Power Voltage The load is too heavy. Check for mechanical binding.
0CA Excess Heat Ambient temperature may be too high. Main power supply board may be damaged. Additional symptom may be a weak motor.
0CB Current Sensor Error Abnormal current sensor off set
0CC Control Voltage Error Shortage of AC. Supply voltage below threshold.
0CD Emergency Stop Relay Error Need to change for mechanical binding.
0CE Drop in control supply voltage This alarm indicates that the voltage of the 24-V input power supply has dropped (24V ? 20%: 19.2V or less).
Check:
(1) Low voltage of the 24-V input power supply
(2) Faulty part inside the controller Action: Check the voltage of the input power supply. If the voltage is normal, please contact IAI.
0D8 Deviation Overflow Please check the mechanical binding. Check moment arm loads (weight & distance). Check for oscillation in the system. May need to adjust Parameter 12 (Positioning Current Limit) from typical of 35% up to a max of 70% (go in 5-10% steps).
0DC Excess Push Movement Range Possible excess movement range during push movement.
0E0 Excess Load Load may be too big. Please check for mechanical binding. If an overload alarm occurs, remove the cause of overload and then resume operation. To reset the overload alarm, input a reset signal from P10. If the alarm must be reset by turning off the main power, wait for a sufficient time (approx. 30 minutes) before resuming operation.
0E4 Encoder Transmission Error This is the transmission error of encoder reception. Either the noise or the reception IC board may have broken down.
0E5 Encoder Reception Error Absolute reset is yet to be performed. Battery error. An absolute reset must be performed after replacing the absolute battery. A disconnected PG cable or poor contact may be the cause. This is a transmission error in the encoder reception IC. Noise may have entered or the reception IC board may be faulty.
0E6 Encoder Counter Error This is the counter error of the encoder. This occurs when number of rotation exceeds 5000 rpm.
0E7 No A, B and Z Feedback Please check the encoder/cable.
0E8 No A and B Pulse Feedback Please check the encoder/cable.
0F9 Abnormal PLD 1) Contact IAI Tech Support to walk-thru initialization procedure of controller. Save parameters and point table first if communication is still active.
2) Check for sources of electrical noise.
3) Controller is damaged inside. May need to replace with new unit. Replacement is new RCP2 system (actuator & controller).
0FA Fixation Memory Breakage Controller initialization memory clear & procedure is needed.
0FB Abnormal CPU CPU shows abnormal movement. Noise may be the cause.
101 Over Run Error (S) Make sure the dip switches for the controllers that are linked all different settings. And also, they must be connected in consecutive sequence. A maximum of 15 controllers plus the main controller can be linked to them.
102 Framing Error (S) Make sure the dip switches for the controllers that are linked all different settings. And also, they must be connected in consecutive sequence. A maximum of 15 controllers plus the main controller can be linked to them.
104 SCI S-QUE OV (S) Receiving external excessive data (during update).
105 SCI S-QUE OV (S) SCI transmission QUE over flow (during update). Also seen when trying to copy a position table with velocity or stroke, etc. values greater than that allowed by the current actuator configuration.
106 Termi R-BF OV (S) Receiving external excessive data (during update).
10A Motorola Sum Error Abnormal update program file (during update).
10B Motorola S Record Error Abnormal update program file (during update).
10C Motorola S Address Error Abnormal update program file (during update).
10D Motorola S File Name Error Abnormal update program file (during update).
10E Timing Limit (W) (S) Please check TEACHInG PENDANT-CPU Base Flash ROM address setting DIP-SW (during update).
10F Timing Limit (E) (S) Please check TEACHInG PENDANT-CPU Base Flash ROM address setting DIP-SW (during update).
111 Timing Limit (P) (S) Please check TEACHInG PENDANT-CPU Base Flash ROM address setting DIP-SW (during update).
112 Input Data Error Input value is irregular. Please input allowable data.
113 Input Under Error Value input is too low. Please input within the allowable data range.
114 Input Over Error Value input is too high. Please input within the allowable data range.
115 Homing Incomplete Prohibited operation is being executed during homing status. First execute homing. Then execute operation.
116 Test Position Data Exist During position addition, first delete or clear the final position data.
117 No Movement Data When movement must be done through the software or teaching pendant, position data is not available.
118 Non-connect Axis Selection Non-connect axis has been selected (there is no error).
119 Teaching pendant Parameter Excess Rotating Number Teaching Pendant internal area parameter allowable rotating number after update has exceeded.
11A Flash Verify Error: S Please check Teaching Pendant-CPU Base Flash ROM address setting DIP-SW.
11B Flash ACK Time Out: S Please check Teaching Pendant-CPU Base Flash ROM address setting DIP-SW.
11C Flash Verify Error: M Please check Teaching Pendant-CPU Base Flash ROM address setting DIP-SW.
11D Flash ACK Time Out: M Please check Teaching Pendant-CPU Base Flash ROM address setting DIP-SW.
11E Pair Data Mismatch Error Please input data with relationships.
11F Absolute Value Under Error The absolute data for input is too low. Please input within the allowable data range.
120 Initial Factor Error The factor input data during controller initialization is abnormal. Please input allowable data.
121 Push Search End Over Excess stroke in the push search end location. Please modify the positioning width.
122 During distribution, multiple axes connection Axis No. distribution must always be executed with a single axis being connected.
180 Axis No. changes is OK (No Error)
181 Controller initialization is OK (No Error).
182 Home change all clear (No Error).
201 Emergency Stop (No Error).
20A Servo OFF during movement Servo was turned OFF during movement.
20C Servo was turned OFF during movement. Start was turned ON during movement. (Hold)
20D During movement, STP-OFF Supply Voltage to the Hold Input before trying to move actuator.
20E Soft Limit Over Soft Limit Over is detected during movement using the Teaching Pendant
301 Over Run Error (M) Please check the number of linked controllers and their sequence.
302 Framing Error (M) Please check the SIO link cable(s) of the primary controller to the sub-linked controllers.
304 SCI R-QUE OV (M) Receiving excessive data.
305 SCI S-QUE OV (M) SCI transmission QUE over flow (during main station mode)
306 Termi R-BF OV (M) Receiving excessive data.
307 Memory Command Breakage Command from the controller is broken now. Due to unknown cause, please record all error list before Teaching Pendant power OFF.
308 Response Time Out Please check the completion for cable controller power ? SIO main station ? subordinate stations.
309 Termi Right Address Error Termi right address unestablished error.
30A Packet R-QUE OV Receiving external excessive data.
30B Packet S-QUE OV Packet transmission QUE over flow
30C No connection error Please check the competition for cable controller ? SIO main station subordinate stations.
This page is wiki editable click here to edit this page.