The first palletizing example works fine under applications that don’t require cycle recovery upon E-stop or power down. The following example uses a “global variable” to maintain the variable count controlling the pallet position increment.
Global variables do not reset after E-stop or power down and thus retain their data until manually cleared. The previous examples used a “local variable” which does reset after E-stop and/or power down. At any rate, both method 1 and method 2 “preload” the previous value of the variables into the corresponding register number and resumes palletizing where it had left off. The best way to accomplish this is to use global variables and flags so that the point on the pallet is retained.
If the pallet is interrupted (i.e. E-stop or power down) the global flag is checked and if it is not off, the pallet did not finish and the pallet position is “preloaded” into the variable. The following method descriptions are exactly the same as the first palletizing example. If you have already read that section you can skip over the two method descriptions.
The first method to control palletizing operations uses the uniform distance between points in the pallet matrix. In an ideal palletizing operation, the distance between columns and rows is the same, however, if they are different it’s just as easy to implement this method. Here’s how the method works:
(Assuming we are moving from left to right on a pallet)
* The first point on the pallet is taught.
1. The distance between columns (and/or rows) is initialized
2. (start loop)
3. The pallet point is moved to in the program.
4. The point data is incremented in the X (column) direction
5. End of row?
6. If not at end of row, loop back up to 1.
7. If at end of row, increment row
8. At the last row?
9. If not at last row, loop back up to 1.
10. If at last row, restart pallet and reset distance, or end program.
This method proves to be very flexible as the distance increment can be altered according to what pallet you are working on. If the pallet size changes, all that needs to be changed in the program is the distance amount and possibly the first point on the pallet. This code will also work on the standard SCARA units that do not have the OFST command available. The problem with this method is that the code is a bit lengthy and extra logic steps must be in place for the position control to occur properly. The next method, using OFST, results in shorter code but may not work with the SCARA (see Scara -> Palletize w/out OFST).
The OFST command allows the user to define a set amount of OFST added on to all points for the moves following the issuance of the OFST command. This OFST setting can be performed on each individual axis or all axes in the system
Which axis actually receives the OFST amount in the point table is determined by the axis pattern placed in Operand 1. The OFST method minimizes code because it adds on to the point table data without actually changing the data in the point table.
For example:
MOVP 1
OFST 10 33.41
MOVP 1
The above code moves the actuators to position 1, adds on an offset in the Y plane of 33.41mm, then moves to position 1 again with an added offset of 33.41 in the Y plane. The X axis remains the same.
If the user wishes to “clear” the offset for the y-axis, the code would look as follows:
OFST 10 0
The following I/O has been chosen by the user:
-- Download this page as a PDF --
Related posts: